Technical FAQs

Ask a Question

What is the difference between Series and Parallel?

 Simple understanding of Series and Parallel Connection

Here is an image that depicts the difference between the two connections. Notice that on a parallel connection the voltage stays the same but the current doubles, and on a series connection the voltage doubles and the current stays the same. 



The recommended way is usually to have a combiner box at the location of the panels, that way there is only a single set of wires that come from the panels into the SCC.
Was this helpful?
What can we do to improve the information ?