Technical FAQs

Ask a Question

What is the Conext ComBox default Username and Password?

Issue:
What is the Conext ComBox default Username and Password?

Product Line:
Conext series accessories

Environment:
Conext ComBox login page

Cause:
User needs to connect to the ComBox

Resolution:
There are two ways to log in to the ComBox. The first way is to log in as an Administrator and the second way is to log in as a User. When the customer logs in as an Administrator, he/she will be able to change settings of the Xanbus connected devices. When the customer connects as a User, he/she will only be able to monitor the devices. 

Logging in as an Administrator:

Username: admin
Password: password 

Logging in as a User:
Username: user
Password: user
Was this helpful?
What can we do to improve the information ?