Technical FAQs

Ask a Question

Can I-line II busway be operated with DC voltages?

Issue:
Can I-Line II busway be operated with DC voltages?

Product Line:
PTLVB - Busways Power IEC & Nema

Environment:
Nema busway sold and supported in the USA.

Cause:
Applicable DC voltages for I-Line busways.

Resolution:
Yes, It can be used with AC or DC voltages up to 600 volts. For Plug-in busway use fully rated 3w and connect to the outside bars. Use appropo DC rated switch or breaker plug-in units .
For Feeder busway use derating info with 4w product. See attached bulletin .


 







CTA-ID : 2036551
Was this helpful?
What can we do to improve the information ?