Technical FAQs

Ask a Question

What is the General recommendations for Generators in XW system?

 General recommendations for generators in XW system


The general recommendations when choosing a generator are:

1) 120/240VAC pure sinewave output (120/208VAC will not work)
2) Unbonded neutral
3) Rated for twice the power of the inverter system
4) Preferably two-wire start if used with AGS

This is because:

1) Inverter will only qualify 120/240VAC generators (L1/L2 180 degrees out-of-phase)
2) Residential systems already bond neutral in Main Service Panel, a second bond in generator will result in dual bond (NEC violation)
3) Takes into account the battery charger plus the loads
4) 2-wire start scenario means the control circuitry is built into the generator, easier to set up for non technical individuals
Was this helpful?
What can we do to improve the information ?