Technical FAQs

Ask a Question

Where can we find more information on the selection of cable pull switch and accessories.

Issue:
All specifications of Preventa Cable Pull Switches product are not published in Digest 176; customers are unsure where to find additional specification and rating information.

Product Line:
All Preventa Cable Pull Switch

Environment:
US product

Cause:
Customers are unsure where to find specification and rating information if it is not in Digest 176

Resolution:
Additional information about ratings and specifications can be found in Preventa Machine Safety Products Chapter 6 catalog which can be downloaded here:  http://download.schneider-electric.com/files?p_Reference=MKTED208051EN-USRev.01Chapter6&p_EnDocType=Catalog&p_File_Id=340584520&p_File_Name=MKTED208051EN-US+Rev.+01+Chapter+6+.pdf

Was this helpful?
What can we do to improve the information ?