Technical FAQs

Ask a Question

What are the catalog numbers for UVR accessories for Powerpact H, J, L breakers?

Issue:
What are the catalog numbers for the field-installable undervoltage (UVR) accessories for Powerpact H, J, and L type circuit breakers?

Product Line:
Powerpact Mold Case Circuit Breaker
 
Resolution:
The catalog numbers are found in the following table:

 
Rated Voltage Factory Installed Cat.Suffix Field installable Cat. No.
AC 24 UK S29404
48 UL S29405
110–130 UA S29406
220–240
208–277 UD S29407
380–480 UH S29408
525–600 UJ S29409
DC 12 UN S29402
24 UO S29410
30 UU S29411
48 UP S29412
60 UV S29403
125 UR S29413
250 US S29414
 
Was this helpful?
What can we do to improve the information ?