Technical FAQs

Ask a Question

MPPT60/80 with different facing arrays.

                                                                                                            MPPT60/80 with different facing arrays


It is generally not a good practice to have different sections of the array facing in different directions dedicated to a single charge controller.
The MPPT will track the maximum power voltage for the array as a whole, however, neither section will be producing to their full potential.
It is best to have a separate controller dedicated to each different facing array.
 
Was this helpful?
What can we do to improve the information ?