Technical FAQs

Ask a Question

Why would you be unable to assign reference 2 channel to LI3 via SoMove light?

Issue:
Unable to assign reference 2 Switching to LI3 via SoMove light.

Product Line:
Altivar 61, Altivar 71

Environment:
Firmware revision 5.8 and later, Somove version 1.9.4.0 and later

Cause:
SoMove will not allow the customer to change Reference 2 switching to LI3.

Resolution:
Ensure that the parameter profile is not set to Not Sepr (Not Separate).  After setting profile to Separate, the customer was able to make the needed change.
 

Was this helpful?
What can we do to improve the information ?