Technical FAQs

Ask a Question

XW AGS starts and stops generator too often

                                                   XW AGS starts and stops generator too often



Some customers attempt to target 50% discharge by setting "30 second start V" to 48V (or 24V for XW4024), not understanding that battery voltage is pulled down under load.
When set up for STOP ABSORB, only 80% of the battery capacity has been replaced. Set 30 second start voltage to 46.6V (23.3 for XW4024), and set "24 hr start V" to 48V (or 24V for XW4024) to more
accurately reflect 50% discharge.
 
Was this helpful?
What can we do to improve the information ?