Technical FAQs

Ask a Question

Where can I find the physical dimensions of the ATV71HD18N4 drive?

ISSUE:
Where can I find the physical dimensions of the ATV71HD18N4 drive?

Product Line:
Al
tivar71 

Environment:
ATV71HD15N4, ATV71HD18N4, ATV71HD11M3X, ATV71HD15M3X
All serial numbers.

Cause:

Physical dimensions of the drive needed prior to purchase.

Resolution: 
The dimensions are Dimensions for the ATV71HD18N4 ( frame size 5B) 
Width = 230mm   9.05in
Height = 400mm   15.75in
Depth = 213mm   8.39in  

(with 1 option card 236mm 9.29in )
(with 2 option cards 259mm 10.20in)
Dimensions can be found in the Altivar 71 installation manual part number ATV71S_installation_manual_EN_1755843_04 and  GLOBAL CATALOG part number 8800CT0501
Was this helpful?
What can we do to improve the information ?