Technical FAQs

Ask a Question

How can you get a preprogrammed CIC card for an Walmart drive?

Issue:
Customer had a Walmart drive that was inoperative and replaced it and got a blank Controller Inside Card.

Product Line:
ATV61

Environment:
Walmart drives

Cause:
Customer had a Walmart drive that was inoperative and replaced it and got a blank Controller Inside Card.

Resolution:
The CIC cards are programmed for Novar or Emerson.
The Wal-Mart CIC cards are sold by Rexel, in Bentonville, Arkansas.
To get a replacement Controller Inside Card, need to contact Bill Marr or Stephen Harrison @ (800) 687-2563.

Was this helpful?
What can we do to improve the information ?