Technical FAQs

Ask a Question

XW charger settings recommendation .

                                                                          XW charger settings recommendation

Different battery chemistries can accept a charge at varying rates. Typically, a FLOODED battery can accept C/5, while a sealed battery, such as gel or AGM
can typically accept C/3. The XW+NA model supports Lithium battery charging (see article FA226500) and also provides a CUSTOM battery menu so charge voltages can be entered manually.
Ultimately, it is the battery manufacturer that must provide the recommendations for charge voltages and charge rate, as a sealed battery can be permanently damaged if overcharged.



 
Was this helpful?
What can we do to improve the information ?