Technical FAQs

Ask a Question

What is the address of the Com Scanner input and Com Scanner output on the ATV61 / ATV71 series drives?

ISSUE:
What is the address of the Com Scanner input and Com Scanner output on the ATV61 / ATV71 series drives?

Product Line:
Altivar 61 / Altivar 71 series drives.

Environment:
All models, All serial numbers.

Cause:
Drive is configured for communication control via the com scanner input and output but the base address of the com scanner input and output is unknown.

Resolution:
The base address of the com scanner input is 12701.
The base address of the com scanner output is 12721.




 

Was this helpful?
What can we do to improve the information ?