Technical FAQs

Ask a Question

What is form Y118 and can it be used with class 8502 contactors and 8536 starters?

Issue: 
What is form Y118 and can it be used with class 8502 contactors and 8536 starters?

Product Line:
NEMA Contactors and Starters

Environment:
NEMA Contactors and Starters

Cause:
Adding a stronger coil for extra power poles.
 
Resolution:
Form Y118 adds a stronger coil to power pole kits for the 8502 or 8536 class unit.
This is not a form for the 8502 or 8536 units, if these are ordered with more than 3 poles they will automatically come with a stronger coil.

Was this helpful?
What can we do to improve the information ?