Technical FAQs

Ask a Question

What is the raw material make up of the 9049A6

Issue:     
What is the raw material make up of the 9049A6

Product Line:
Pressure Switches

Environment:
Class 9049 pressure switch accessories

Cause:
What is the raw material make up of the 9049A6
 
Resolution:
There are 2 brass part in this kit.

The rod is Alloy #330 brass, composition is as follows:

 

Cu        65 to 68%

Zn        33.5%

Fe        0.07%

Pb        0.2 - 0.8%

 The brass stud is Alloy # 360 brass (stud that connects two or more rods into a longer rod).  Composition is as follows:

 Cu        60-63%

Pb        3.5 - 3.7%

Fe        0.35%

Zn        Remainder

 The rod stops and locking screws are Cold Rolled Steel.

 The float is #304 stainless.

 

Was this helpful?
What can we do to improve the information ?