Technical FAQs

Ask a Question

What is the recommended line reactor for using a 1 phase input 3 phase output ATV61HD37M3X on a 25HP motor?

 Issue:
What is the recommended line reactor for using a 1 phase input 3 phase output ATV61HD37M3X on a 25HP motor?
 
Product Line:
Altivar ATV61 1 phase input 3 phase output only
 
Environment:
All 
 
Cause:
Line reactor for surge suppression when using 1 phase input 3 phase output. 
 
Resolution:
The recommended 5%  line reactor is 
RL16002  ( open type)
RL16012 (Line reactor in NEMA 1 box)
 
Was this helpful?
What can we do to improve the information ?