Technical FAQs

Ask a Question

Can I replace a ATV61WU55N4U with an standard ATV61HU55N4U?

Issue:
Can I replace a ATV61WU  with an ATV61HU ? 

Product Line:
ATV61W

Environment:
All

Cause:
None

Resolution:
The ATV61W is a self contained NEMA 12 enclosed drive.  The drive inside the 61W is not a standard drive.  The drive is an ATV61H modified for this enclosure. Therefore the answer to the ATV61H replacing the ATV61W is no.  This is not an option.
Was this helpful?
What can we do to improve the information ?