Technical FAQs

Ask a Question

How many logic inputs are on the ATV32 drive?

Issue:
How many logic inputs are on the ATV32 drive?
 
Product Line:
Altivar 32
 
Environment:
All 
 
Cause:
logic input assignments option
 
Resolution:
There are 6 logic inputs on the ATV32 drive.
 
Was this helpful?
What can we do to improve the information ?