Technical FAQs

Ask a Question

Where can I receive support writing a program for my optional IMC card installed in an Altivar 61 or Altivar 71 Drive?

ISSUE:
Where can I receive support writing a program for my optional IMC card installed in an Altivar 61 or Altivar 71 Drive?

Product Line:
VW3A3521 IMC card. (Used only in ATV61 / ATV71 series drives).

Environment:
All models, All serial numbers.

Cause:
Assistance needing writing a program for the IMC card for a custom application.

Resolution:
Custom IMC programming assistance is available through our Application Design Engineering group.  Contact your local distributor to be placed in touch with this group.  Your local distributor will contact their OEM sales representative to engage the Application Design Engineering group.
Was this helpful?
What can we do to improve the information ?