Technical FAQs

Ask a Question

Can a PHG36030G be retrofitted with a HJL36060 breaker at 60 amps . Also, can a PHG36100G be retrofitted with a 200a JJL breaker?

Issue:
Can a PHG36030G be retrofitted with a HJL36060 breaker at 60 amps . Also, can a PHG36100G be retrofitted with a  200a JJL breaker?

Product Line:
I-Line Busway

Environment:
Breaker Bus Plugs

Cause:
Maintenance/Cross Reference

Resolution:
Yes,  an HJP36060 or HJL36060 or similar can fit in place of a 30a breaker . Labels are the only issue . Also, a JJP36200 or JJL36200 can be interchanged. Both Powerpact H and J breakers use the same size bus-plug box.

Was this helpful?
What can we do to improve the information ?