Technical FAQs

Ask a Question

Can I use the VW3A1101 keypad to copy a program from one ATV32 to another ATV32 drive?

Issue:
Can I use the VW3A1101 keypad to copy a program from one ATV32 to another ATV32 drive?

Product Line:
Altivar 32

Environment:
All

Cause:
Needs a quick way to copy the ATV32 program from one drive to the next.

Resolution:
Yes you can use the VW3A1101 keypad to copy the ATV32s program from one drive to the identical ATV32 drive.
Note you will also need a cable and a RJ45 to RJ45 female conjunction port.
Cable part number 1 meter is VW3A1104R10
RJ45 to RJ45 female port is VW3A1105  or you can use the VW3A1101 remote mounting bezel kit part number VW3A1103.

Was this helpful?
What can we do to improve the information ?