Technical FAQs

Ask a Question

XW SCP battery level indicator accuracy

                                                                                                                                                                                                            XW SCP battery level indicator accuracy








Graph is more accurate when discharging than when charging. When new charge cycle is initiated, bar graph will show low state, and only show full when Absorption stage has completed.
IF CUSTOMER COMPLAINS BATTERY LEVEL INDICATOR IS CYCLING, MAKE SURE RECHARGE VOLTS IS NOT SET TOO HIGH, OR SET TOO CLOSE TO GRID SUPPORT VOLTAGE








Was this helpful?
What can we do to improve the information ?