Technical FAQs

Ask a Question

What is the part number for the control card kit for An ATV61 drive frame size 9 through 15?

Issue:
What is the part number for the control card kit for An ATV61 drive frame size 9 through 15?

Product line:
Altivar 61 series

Environment:
Frame size 9-15, all serial numbers.

Cause:
Replacement part number needed.

Resolution:
The part number for the ATV61 control card for frame size 9-15 (>=90KW) is VX4A61101Y
Was this helpful?
What can we do to improve the information ?