Technical FAQs

Ask a Question

Will the control board terminal blocks from the ATV58 fit into the ATV61 or ATV71 drives?

Issue:
Will the control board terminal blocks from the ATV58 fit into the ATV61 or ATV71 drives?

Product Line:
ATV58, ATV61, ATV71

Environment:
All models, all serial numbers

Cause:
Customer wants to save time instead of rewiring all the terminals.

Resolution:
No, the Altivar 58 drive parts are not compatible with ATV61 or any other Altivar drive.
Was this helpful?
What can we do to improve the information ?