Technical FAQs

Ask a Question

How do I set the battery bank voltage on a TM500?

Setting the Voltage Level of the TM500

 

1A. Press the SELECT button until the Voltage LED ( V ) is illuminated.

2A. Press the SELECT and RESET buttons simulataniously until the LED display flashes.

3A. Press the RESET button to change the displayed voltage to the desired fully-charged voltage level:

• For a 12 VDC system, set this voltage between 14.3–14.9 volts for

lead-acid batteries.

• For a 24 VDC system, set this voltage between 28.6–29.6 volts for

lead-acid batteries.

• For a 48 VDC system, set this voltage between 57.2–59.2 volts for

lead-acid batteries.

Refer to the battery manufacturer’s recommendation for other types

of batteries.

4A. Press the SELECT button to accept the new value. The selection range is between 10 to 64.9 VDC.

Was this helpful?
What can we do to improve the information ?