Technical FAQs

Ask a Question

Why is my SW Plus 5548 Faulting with over current condition when it starts a Bulk Charge?

Over Current Condition on the Trace SW and SW Plus Series 

The over current condition on the Trace SW and SW Plus is commonly caused by having too much AC load, or a short circuit condition on the SW output.

If output wires are removed by a qualified person, and the overcurrent condition cannot be cleared, remove AC and DC for 20 minutes.
If the overcurrent condition does not clear, the SW will need be repaired or replaced.

Call into Technical Support for the Authorized Service Center near you.
866-519-1470
Was this helpful?
What can we do to improve the information ?