Technical FAQs

Ask a Question

What is the enclosure frame size for and Class 8638 Type 22FHA4Y with modification X10?

Issue:
Difficulty in finding out the enclosure size.

Product Line:
Enclosed ATS22 Soft Start

Environment:
863822FHA4Y with modification X10

Cause:
None

Resolution:
Recommended using Table 12 on page 35 manual 30072-453-26
863822FNA4Y X10 - This is a Y05 (integrated bypass), 50 deg C (option X10), 100 hp, 460v = size D (use column 2 of Table 12, pg 35)
 

 
Was this helpful?
What can we do to improve the information ?