Technical FAQs

Ask a Question

What is the padlock attachment for Powerpact R frame circuit breakers?

Issue:
What is the padlock attachment for the Powerpact R Frame breakers

Product Line:
Powerpact R frame

Environment:
Products sold in North America

Cause:
Need to place a padlock on the Powerpact R Frame breaker in order to restrict the operation of the breaker.

Resolution:
Removable (lock OFF only) - S33996
User-added image

Fixed (Lock OFF or ON) - S32631
User-added image

Fixed (Lock OFF only) - MPRPAF
User-added image

Instruction Bulletin

Removable Padlock Attachment for R-frame and NS1600b-NS3200 Circuit Breakers
http://download.schneider-electric.com/files?p_File_Id=74200585&p_File_Name=48049-247-02.pdf

MPRPAF and S32631 Fixed Padlock Attachment Kits (S32631–ON/OFF orMPRPAF–OFF Only) for PowerPact™ L, M-, P-, and R-Frame and Compact™ NS630b–NS320 Circuit Breakers
http://static.schneider-electric.us/docs/Circuit%20Protection/Molded%20Case%20Circuit%20Breakers/3000%20A%20Frame%20PowerPact%20R/Accessories/48049-246-02tri.pdf

Keyword:
RGA RGF RJA RJA RKA RKF RLA RLF

Was this helpful?
What can we do to improve the information ?