Technical FAQs

Ask a Question

Does Schneider Electric offer a momentary action cable pull switch that is UL/CSA certified?

Issue:
Does Schneider Electric offer a momentary action cable pull switch that is UL/CSA certified?

Product Line:
Cable Pull Switches

Environment:
XY2CE Cable Pull Switches, excludes XY2CE Switches with pilot light.

Cause:
Clarify the certification of the XY2CE switch when multiple documents contradict weather the device is UL certified.

Resolution:
The XY2CE momentary cable switches without a pilot light are UL certified.  Link below states the certifcation of the XY2CE family.
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=NKCR.E164353&ccnshorttitle=Auxiliary+Devices&objid=1074106764&cfgid=1073741824&version=versionless&parent_id=1073990247&sequence=1

Was this helpful?
What can we do to improve the information ?