Technical FAQs

Ask a Question

MFlex - Why does the product selector not allow NEMA rated contactor option?

Issue:
Product selector will not allow NEMA rated contactors

Product Line:
M-Flex

Environment:
Engineered Features

Cause:
None

Resolution:
Available for Barriered design configurations only; requires selection of Power Circuit S, Z, T, or R

Was this helpful?
What can we do to improve the information ?