Technical FAQs

Ask a Question

What are the voltage and HP ranges for the ATV31C drive?

Issue:
Is there an option for 240vac 3 phase input and 3 phase output on the ATV31C drives?

Product Line:
Altivar ATV31C

Environment:
only ATV31C

Cause:
Needs to know if there is an option for 240vac 3 phase input 3 phase output.

Resolution:
There is not an option for 240vac 3 phase input and 3 phase output.  
The ATV31C offers 1 phase input 240vac and 3 phase 240vac output .25HP to 3HP.
The ATV31C offers 3 phase input 480vac and 3 phase 480vac output  .5HP to 20HP.

Reference  the atv31c_installation manual_EN_V3
 

Was this helpful?
What can we do to improve the information ?