Technical FAQs

Ask a Question

How do I connect the AGS to my HoneyWell HW7000EH?

This particular Generator does not have a remote connection. If approved by HoneyWell, we can piggyback to the switch panel wires and simulate the connection using the AGS' relays. 


- Generator Type: Type 8

- Wires Needed on AGS Harnes:

13,14,16, 17, 18

  * Wires 13, 16, 18 get connected together

- Wire 14 goes to the "Black" wire that     connects to the Ignition Coil

- Wire 17 gets connected to the "Black / White" cables that controls the Starter Motor

- Wire 13, 16 & 18 go connected to the "White" wire that connects to the battery positive of the unit (+12VDC)

Wiring diagram found page 13 on link:
https://www.gardnerinc.com/manuals/pdf/ipl/Honeywell%20generators/Service%20Manuals/HW7000EH/102141_HW7000EH_SERVICE_MANUAL.pdf



Was this helpful?
What can we do to improve the information ?