Technical FAQs

Ask a Question

Why is my Conext SW displaying a warning W69?

W69- AGS Not Connected 

On the Conext XW inverter, either the SW2524 or the SW4024, if the unit is faulting or showing a warning W69 is because the inverter is looking for an XW AGS. This warning is caused by the inverter having the "GEN SUPPORT" features is enabled but no AGS is connected to the Xanbus communication. To resolve the issue, please disable the Gen Support capability under Advance Settings of the CSW menu using SCP. 
Was this helpful?
What can we do to improve the information ?