Technical FAQs

Ask a Question

C-series overcharging batteries in diversion mode

 C-series overcharging batteries in diversion mode






Verify load terminals read the same as battery voltage once BULK voltage is reached (5 blinks green). 
If so, and the battery voltage still climbs above the BULK setting, it is likely the dump load has opened up. 










 










 
 
 
Was this helpful?
What can we do to improve the information ?