Technical FAQs

Ask a Question

What is the basic setup for ATV61 and METASYS N2 card?

Issue:
What is the basic setup for ATV61 and METASYS N2 card?

Product Line:
ATV61/71

Environment:
All range, All serial number

Cause:
Need to commission the ATV61 N2 card.

Resolution:
Set the following parameters in the drive:
Address: Customer supplied
Baud rate: 9600 or other
Format: 8N1
Timeout: 60 sec
After setting the parameters, check the Frame Counter in Communication Map to see if it is counting and Error Frame counter should be 0. The 2.1 LED flashes intermittently.

Was this helpful?
What can we do to improve the information ?