Technical FAQs

Ask a Question

mounting space for the LC and LJ breakers

Issue:
What is the mounting space difference between the LC, LI, and LXI breakers and the Powerpact L Frame breakers?

Product Line:
I-LINE Breakers

Environment :
Products sold and used in the United States

Cause:
Selecting breakers for a I-LINE panel.

Resolution:
The LC, LX, and LXI breakers take 7.5 in of mounting height.
The LD, LG, LJ, LL, and LR take 6.0 in of I-LINE mounting height.

Found on page 9-34 in Digest 177, Table 9.99: Circuit Breaker / Sub-feed Lug Kit Mounting Space Requirement
http://download.schneider-electric.com/files?p_Doc_Ref=0100CT1501_SEC-09
Was this helpful?
What can we do to improve the information ?