Technical FAQs

Ask a Question

Do your single phase grid tie inverter come with DC/AC Disconnect Switches (GT / TX series inverters)

 The wiring box includes a 600 V utility/PV disconnect switch that switches both AC and DC at the same time.
Depending on the installation, an external AC and/or DC disconnect might be required if the Inverter is installed in a location not easily accessible to utility or fire personnel. Consult local authorities for additional information.
Was this helpful?
What can we do to improve the information ?