Technical FAQs

Ask a Question

PV30 and PV45 error / fault code 0 X 80

This fault is not listed in the user guide. It is the "stop switch fault" on the front panel, all that is needed is to turn the switch to ON.
Was this helpful?
What can we do to improve the information ?