Technical FAQs

Ask a Question

Phase rotation for PV inverters

The PV100S,P,H and the PV225S,P must have clock wise phase rotation.

If the local utility has counter-clockwise rotation, two of the phases must be reversed to accomplish the clockwise phase rotation.

Any inverter that's uses the DSP board can do auto rotation detection.
That is from the PV45208 down
Was this helpful?
What can we do to improve the information ?