Technical FAQs

Ask a Question

Batteries - How many batteries do I need?

How many batteries do I need?

There are a few factors that need to be considered before you determine the quantity of batteries needed. First, consider the type of battery you intend to use with your application. Next, determine the size of the battery and the number of amp hours you require between charge cycles. Most people have a 400-450 amp-hour battery bank, but this depends on use of your system.
Was this helpful?
What can we do to improve the information ?