Technical FAQs

Ask a Question

Batteries - what type should I use?

What type of batteries should I use in my Inverter/Charger installation?

Schneider Electric recommend using only high-quality deep cycle batteries in Wet, Gel or AGM (Absorbed Glass Matt) technologies to be used with Schneider Electric products. Deep-cycle batteries are designed specifically for a deep discharge and a rapid recharge. Wet cell batteries include 6-volt (golf cart) batteries and require some maintenance. Gel cell batteries and AGM batteries are sealed and typically require very little maintenance. Do not use starting batteries for inverter applications.
Was this helpful?
What can we do to improve the information ?