Technical FAQs

Ask a Question

Batteries - What is Three-Stage Charging?

What is Three-Stage Charging?

Multistage charging ensures batteries receive optimum charging, but with minimal wear and tear, regulating the voltage and current delivered to the batteries in three automatic stages:

Bulk: Replaces 70-80% of the battery's state of charge at the fastest possible rate.

Absorption: Replenishes the remaining 20-30% of charge, bringing the battery to a full charge at a slow, safe rate.

Float: Voltage is reduced and held constant in order to prevent damage and keep batteries at a full charge.
Was this helpful?
What can we do to improve the information ?