Technical FAQs

Ask a Question

Net metering - Why is it important?

Why is net metering important?

There are three reasons net metering is important.
First, as increasing numbers of residential and small commercial customers install renewable energy systems in their homes, there needs to be a simple, standardized protocol for connecting their systems into the electricity grid that ensures safety and power quality.
Second, many residential customers are not at home using electricity during the day when their systems are producing power, and net metering allows them to receive full value for the electricity they produce without installing expensive battery storage systems.
Third, net metering provides a simple, inexpensive, and easily-administered mechanism for encouraging the use of renewable energy systems, which provide important local, national, and global benefits.
Was this helpful?
What can we do to improve the information ?