Technical FAQs

Ask a Question

Off Grid Systems - are they difficult to operate and maintain?

Are these systems difficult to operate and maintain?

No, they are very simple. You do need to monitor power usage and ensure that your batteries are receiving adequate recharge, this is done with the aid of a simple-to-understand system status meter. Batteries require some maintenance, water must occasionally be added and connections cleaned and retightened. PV modules may also require annual washing.
Was this helpful?
What can we do to improve the information ?