Technical FAQs

Ask a Question

Backup - How is the system recharged?

How is the system recharged?

Xantrex backup systems recharge themselves automatically whenever utility power is available. To be able to recharge the system during a power outage, a propane-, natural gas- or diesel-powered generator can be included in the system. Xantrex SW (sine wave) inverters can automatically start and stop a generator as needed during long outages. All Xantrex systems can also be recharged using renewable energy sources such as solar panels.
Was this helpful?
What can we do to improve the information ?