Technical FAQs

Ask a Question

Backup - How do I decide which system is right for me?

How do I decide which system is right for me?

For protection from long outages, include a generator or solar panels in your Xantrex system. Shorter outages can be handled by a battery-only system. Solar panels are significantly more expensive than a generator, but can provide year-round electric bill savings and require no fuel or maintenance.

Xantrex top-of-the-line systems, using sine-wave SW Series inverters, come in three power output levels and integrate easily with a generator for automatic starting and system recharging. Several lower-cost Xantrex systems are intended primarily as battery-only systems. Your Xantrex dealer can help you select the system that best meets your needs and answer any additional questions.
Was this helpful?
What can we do to improve the information ?