Technical FAQs

Ask a Question

What is the ferrite core for on the GT3.8?

When stacking more than 1 GT3.8 using the Xanbus ports, it is necessary to install the ferrite on the Xanbus cord to maintain FCC class B listing. The attached installation sheet ships with the GT3.8.
Was this helpful?
What can we do to improve the information ?