Technical FAQs

Ask a Question

04J Bulk/EQ Timer SWPLUS

Some customers will note that the SWPLUS bulk/EQ timer will not increment when in EQ.

If in bulk, it increments when the voltage is above nominal. In EQ it increments when the voltages is .5 volt below EQ set point at 24 VDC, or 1 volt below EQ set point at 48 VDC. Timer resets to zero when bulk flag is set (new bulk cycle).
Was this helpful?
What can we do to improve the information ?