Technical FAQs

Ask a Question

GTView running on a MAC

GTView, as it stands right now, is only functional on the PC platform. That said, we have published the RS232 command set http://www.xantrex.com/web/id/1626/docserve.asp so that if a MAC programmer would like to take the initiative, he can.
Was this helpful?
What can we do to improve the information ?