Technical FAQs

Ask a Question

THD for DR series

Some people may want to know what the THD is for the DR series. This is not really relevant because it is modified sine wave, but here is the answer.

Model,THD,highest single harmonic distortion

DR1512, 37.1%, 25%
DR1524, 27.4%, 26%
DR2412, 37.3%, 30%
DR2424, 29.9%, 24%
DR3624, 37.6%, 31%
Was this helpful?
What can we do to improve the information ?